The ultra-small, extreme power density Gold Twitter servo drive will be available with an enhanced version, including a capability to be powered from single power source

Petah-Tikvah, Israel– January 1, 2019 Elmo Motion Control (Elmo), a leading provider of advanced motion solutions, announces a new enhanced Gold-Twitter version with single source up to 95VDC.  This will allows users to use a single source power for both, the drive and logic power.

 

As part of its continues engineering efforts, the Elmo R&D team was able to integrate a higher voltage internal supply into the ultra-small Gold Twitter. Gold Twitter 80V and 100V versions denoted with a new P/N suffix can now operate from a single power supply. VL (Control Supply) and VP+ (Power Supply) operating from a single source is a huge benefit for machine builders. The single control supply topology contributes to lower EMI, and reduced sensitivity to poor external wiring.

Despite the changes the new enhanced version will be completely F3 compliant. The strict compliance with the F3 rules (Fit, Form, and Function) ensures transparent usage for customers that currently use G-TWI.

 

For ordering the single power supply G-TWI, add the suffix “S” to the part number. For example: G-TWIR80/80EES.       Click here to read more.

About Elmo Motion Control

Elmo Motion Control – a leading manufacturer of advanced servo and motion technologies– offers intelligent, high power-density servo drives and motion controllers for more than 30 years. Elmo’s award-winning ultra-small drives and multi-axis controllers enhance overall machine precision, speed, and ensure a fast, real-time responses for any application. Controlled by the Elmo application studio (EAS)—a software environment that cuts integration time and maintenance costs—Elmo’s servo technology improves machine performance, minimize machine footprint and cabling, improve throughput, and give OEMs a competitive edge. Founded in 1988, the company is headquartered in Israel, employs more than 300 staff worldwide, and has a dedicated presence in the United States, China, Germany, Italy, Korea, Poland and the United Kingdom. For more information, visit www.elmomc.com